CIMPLICITY REST API Web Service
CIMPLICITY REST API Web Service / CimDataItem Json Schema
CimDataItem Json Schema
Description
is an object that represents a dataitem of an object.
Overview
CimDataItem
is an object that represents a dataitem of an object.
ID : string
is a string containing the name of the data item as defined in the class.
IsJIT : boolean
is a boolean indicating if the data item is Just-In-Time. The class defines how this is set.
OPCUA_NodeID : string
is the NodeID in the CIMPLICITY OPC UA Server that represents this data item.
PointID : string
is a string containing the point ID for the object corresponding to the classes data item.
Properties
NameDescriptionData Type
is a string containing the name of the data item as defined in the class.string
is a boolean indicating if the data item is Just-In-Time. The class defines how this is set.boolean
is the NodeID in the CIMPLICITY OPC UA Server that represents this data item.string
is a string containing the point ID for the object corresponding to the classes data item.string
See Also